Technical FAQs

Ask a Question

Is a Padlock Attachment available for the GJL?

Yes. Use the AHP to lock breaker. The AHP locks in OFF position only.
Suitable for padlock with a shaft diameter up to 0.312 in. (8 mm).

CTA-ID : 5969
Was this helpful?
What can we do to improve the information ?