Technical FAQs

Ask a Question

What are the ratings for the AAC Alarm Switch for the GJL?

The ratings for the AAC are: 3A-600 Vac, 6A-480 Vac, 0.3A-250 Vdc, 0.8A-125 Vdc


CTA-ID : 5966
Was this helpful?
What can we do to improve the information ?