Technical FAQs

Ask a Question

What are the ratings for the AAC 1a1b aux switch contacts for the GJL Circuit Breaker?

Per Digest, ratings are: 3A-600 Vac, 6A-480 Vac, 0.3A-250 Vdc, 0.8A-125 Vdc.


CTA-ID : 5965
Was this helpful?
What can we do to improve the information ?