Technical FAQs

Ask a Question

Is the replacement pilot light bulb available for the 2510 KF1A?

This is a sealed unit, complete module part number 9999 PL11 for Red or 9999 PL11G for Green must be replaced.

This also applies to 2510 KF3A, 2510 KG1A, 2510 KG3A, 2510 KG5A, 2510 KGJ1A, 2510 KGJ3A, 2510 KO1A, 2510 KO1AT, 2510 KO2AT, 2510 KO3A, 2510 KO5A, 2510 KS1A, 2510 KS3A, 2510 KSJ1A, 2510 KSJ3A, 2511 KF11A, 2511 KF22A, 2511KG11A, and 2511 KG22A.


CTA-ID : 4561
Was this helpful?
What can we do to improve the information ?