Technical FAQs

Ask a Question

Where do you hook up a speed potentiometer on the Altivar ATV18 unit?

Issue:  Where do you hook up a speed potentiometer on the Altivar ATV18 unit?
 
Product Line:  ATV18
 
Environment:  All
 
Cause:  Potentiometer wiring
 
Resolution:  Connect the high side of the pot to +10;
the wiper to Anaolg Input 1 (AI1);
the low side of the pot to Common.


 
Was this helpful?
What can we do to improve the information ?