Technical FAQs

Ask a Question

Does the Altivar ATV18 drive offer `Machine Speed` functionality.

Issue: Does the Altivar ATV18 drive offer `Machine Speed` functionality.
 
Product Line: ATV18
 
Environment: All
 
Cause: N/A
 
Resolution: This unit does not as there are no programmable output process displays available on these drives. Can do it with ATV56 / 66.



 
Was this helpful?
What can we do to improve the information ?