Technical FAQs

Ask a Question

Is the Altivar ATV16 DB Resistor kit listed under UL, IEC, etc.?

Issue: Is the Altivar ATV16 DB Resistor kit listed under UL, IEC, etc.?
 
Product Line: ATV16
 
Environment: All
 
Cause: Certification
 
Resolution: ATV16 is UL, CSA, IEC, and VDE listed. All components of ATV16 when used in conjunction with the drive come under the same listings.


 
Was this helpful?
What can we do to improve the information ?