Technical FAQs

Ask a Question

What`s the max. continuous current output of the DC Power Supply on the Altivar ATV16 because customer wants to power some sensors along with the forward / reverse signals?

The max output current for the ATV16 24V supply is 60mA. This is intended for the drives` control inputs only. Using external sensors could blow this supply if they shorted out. For this reason we do not recommend doing so.


CTA-ID : 4286
Was this helpful?
What can we do to improve the information ?