Technical FAQs

Ask a Question

How do the fault contacts work on the Altivar ATV16?

Issue: How do the fault contacts work on the Altivar ATV16?
 
Product Line: ATV16
 
Environment: All
 
Cause: N/A
 
Resolution: They change states when the unit is powered up, then they change states again upon a fault or loss of power.


 
Was this helpful?
What can we do to improve the information ?