Technical FAQs

Ask a Question

How do you wire the start and stop on the 3 wire option board for the Altivar ATV16?

Issue: How do you wire the start and stop on the 3 wire option board for the Altivar ATV16?
 
Product Line: ATV16
 
Environment: All
 
Cause: Control wiring
 
Resolution: Wire the stop between the +24 and LI1, start goes between +24v and FW or +24v to RW for reverse direction.


 
Was this helpful?
What can we do to improve the information ?