Technical FAQs

Ask a Question

What is the maximum distance the Altivar ATV16 keypad can be remotely mounted.

Issue: What is the maximum distance the Altivar ATV16 keypad can be remotely mounted.
 
Product Line: ATV16
 
Environment: All
 
Cause: N/A
 
Resolution: We provide a 3 meter ( aproximately 10 feet ) cable which is the maximum available. The quality of the cable determines how much longer the cable can be but we do not support it.


 
Was this helpful?
What can we do to improve the information ?