Technical FAQs

Ask a Question

Can I use a Capacitive Start motor on the Altivar ATV16 drive?

Issue: Can I use a Capacitive Start motor on the Altivar ATV16 drive?
 
Product Line: ATV16
 
Environment: All
 
Cause: N/A
 
Resolution: A capacitive start motor cannot be used on the out put of the drive because the device will appear as a short to the drive and the drive will trip on short circuit.


 
Was this helpful?
What can we do to improve the information ?