Technical FAQs

Ask a Question

Why will the Altivar ATV16 not run when set up for local mode?

Issue: Why will the Altivar ATV16 not run when set up for local mode?
 
Product Line: ATV16
 
Environment: All
 
Cause: Not running in local
 
Resolution: Verify Fwd command and correct switch positions as well as verify reference frequency. Need to set LFr to the required setting.


 
Was this helpful?
What can we do to improve the information ?