Technical FAQs

Ask a Question

What will cause the reS, StS & StE parameters to go back to off on the Altivar ATV16 and what occurs if sw. 2 is in off position?

Issue: What will cause the reS, StS & StE parameters to go back to off on the Altivar ATV16 and what occurs if sw. 2 is in off position?
 
Product Line: ATV16
 
Environment: All
 
Cause: Parameters resetting
 
Resolution: If someone changed the sw. 2 on back of keypad the parameters would go back to default settings and the operation of switch 2 changes unit between local versus terminal command.


 
Was this helpful?
What can we do to improve the information ?