Technical FAQs

Ask a Question

Is the 9001 K60 padlock attachment plastic and stainless steel?

Yes. If it says it can be used with an 9001 SK operator the steel parts are stainless steel.


CTA-ID : 5136
Was this helpful?
What can we do to improve the information ?