Technical FAQs

Ask a Question

What is the 24 volt replacement coil for a Type SA NEMA size 00 contactor or starter?

The 24 vac replacement coil for all Size 00 contactors depends on the device`s series or revision. The following outlines the part by Series number: Series A 60hz - 31041-400-20, Series A 50hz - 31041-400-22, Series B - 9998SAC23. For enclosed devices, the series information is based on device and not enclosure nameplate.

CTA-ID : 4805
Was this helpful?
What can we do to improve the information ?