Technical FAQs

Ask a Question

Do you have +/- speed option on the Altivar ATV16 drive?

Issue: Do you have +/- speed option on the Altivar ATV16 drive?
 
Product Line: ATV16
 
Environment: All
 
Cause: N/A
 
Resolution: You would need the Material handling option card and the PC option. You need to change the setting on the Material handling card with the PC option.


 
Was this helpful?
What can we do to improve the information ?