Technical FAQs

Ask a Question

Why is the Altivar ATV16 local light flashing and it is not responding to terminal commands?

Issue: Why is the Altivar ATV16 local light flashing and it is not responding to terminal commands?
 
Product Line: ATV16
 
Environment: All
 
Cause: Local LED flashing
 
Resolution: Need to change switch one on the back of the keypad to off for terminal command. The local light flashing indicates set up for local keypad control.


 
Was this helpful?
What can we do to improve the information ?