Technical FAQs

Ask a Question

Why is Altivar ATV16 only going to 50 hz and want 60hz maximum frequency?

Issue: Why is Altivar ATV16 only going to 50 hz and want 60hz maximum frequency?
 
Product Line: ATV16
 
Environment: All
 
Cause: Speed won't go above 50Hz
 
Resolution: Need to set TFR ( maximum freqeuncy ) for 60 and HSP ( high speed ) to 60hz.


 
Was this helpful?
What can we do to improve the information ?