Technical FAQs

Ask a Question

How many preset speeds are possible with the general use option card for the Altivar ATV16.

Issue: How many preset speeds are possible with the general use option card for the Altivar ATV16.
 
Product Line: ATV16
 
Environment: ATV16 with gen use option card
 
Cause: N/A
 
Resolution: There are 4 available:Preset speed 1 when both LI2 and LI3 are low.  The speed will be LSP or the analog input speed reference.  Preset speed 2 when both LI2 and LI3 are high.  The speed will be the HSP setting.  Preset speed 3, when only LI2 is high.  The speed will be the 3SP setting.  Preset speed 4 when only LI3 is high.  The speed will be the 4SP setting.  A run command on LI1 will always have to be present for the drive to run at any of these speeds.


 
Was this helpful?
What can we do to improve the information ?