Technical FAQs

Ask a Question

How can you wire the Altivar ATV16 drive to run it at one speed without a pot?

Issue: How can you wire the Altivar ATV16 drive to run it at one speed without a pot?
 
Product Line: ATV16
 
Environment: All
 
Cause: N/A
 
Resolution: Need to jumper +10 to AIV, and then adjust HSP to the desired speed and as long as have a direction signal made and not fault present unit will run at HSP..


 
Was this helpful?
What can we do to improve the information ?