Technical FAQs

Ask a Question

Is there a way to store the Lfr setting after power is recycled on the Altivar ATV16?

You can run the drive in Terminal mode, jumper +10 to AIV and then adjust HSP parameter to control the speed. This will work similar to adjusting Lfr except the value will be stored after power is recycled which can not be done in LFR paramer which reverts back to zero when cycle power.

CTA-ID : 4251
Was this helpful?
What can we do to improve the information ?