Technical FAQs

Ask a Question

Why is the Forward light blinking and will not allow changes to the programming of the drive?

The unit has been given a start command but no speed reference is present.  When the drive is in a run state, you cannot make changes to the programming.  Remove the control wiring (start signal) and try to program it again.


CTA-ID : 4241
Was this helpful?
What can we do to improve the information ?