Technical FAQs

Ask a Question

Can we use a 2 1/4`` mushroom knob on the 9001 KR9, SKR9, KR8, or SKR8 push pull mushroom button?

Yes. Use the illuminated mushroom knob, 9001 *21, * indicate color, and a 9001 K54 adapter. This will void Type 6 rating.


CTA-ID : 5086
Was this helpful?
What can we do to improve the information ?