Technical FAQs

Ask a Question

Are the option cards obsolete for the Altivar ATV16 drives?

Issue: Are the option cards obsolete for the Altivar ATV16 drives?
 
Product Line: ATV16
 
Environment: All
 
Cause: Options
 
Resolution: Yes, the entire family is obsolete


 
Was this helpful?
What can we do to improve the information ?