Technical FAQs

Ask a Question

Where should the wires for meter kit 52902-020-50 be connected to the Omegapak 8804 Type PT drive?

Connect the +V terminal on the meter (Red wire) to terminal 17 (+10 VDC) on the main control board.
Adjust the P1 potentiometer on the back of the meter to calibrate.

CTA-ID : 4217
Was this helpful?
What can we do to improve the information ?