Technical FAQs

Ask a Question

How is a 9001 K2105 potentiometer wired?

There are 3 terminals. The center terminal is the wiper. The outside 2 are each end of the potentiometer. You wire to the center tap and either end depending on whether you want the resistance to increase or decrease.


CTA-ID : 5064
Was this helpful?
What can we do to improve the information ?