Technical FAQs

Ask a Question

Can the Omegapak 8804 PT frequency be increased above 60 hz?

R86 is a snip out resistor. With this removed, the max speed will go up to 90 hz. Adjust the high speed with potentiometer P3.


CTA-ID : 4210
Was this helpful?
What can we do to improve the information ?