Technical FAQs

Ask a Question

Does the jumper from 7 to 16 also come out when removing the speed pot from a Omegapak 8804 PT15GG4, which is landed to pins 7,15,and 17?

Yes. Remove that jumper also.


CTA-ID : 4207
Was this helpful?
What can we do to improve the information ?