Technical FAQs

Ask a Question

What is the service bulletin part number of the Type MC-24 (Type PT Controller - Mod S08 {part number 52011-425-50}) stepped reference option board for use with Power Transistor ( Type PT) Omegapak 8804?

8804-53 is the part number of the manual.

CTA-ID : 4203
Was this helpful?
What can we do to improve the information ?