Technical FAQs

Ask a Question

What is the instruction sheet part number of the Type SR-01 120 volt AC start relay for use with 460v,Type VT, CT and PT Omegapak 8804?

8804-SR-01 is the part number of the manual.


CTA-ID : 4200
Was this helpful?
What can we do to improve the information ?