Technical FAQs

Ask a Question

What contacts do we add to a 9001K35 to get contacts closed when joystick is in the center position?

We have no contacts that will be closed in the center position. The cams in the joystill hold all contacts open in the center position. Suggest using relays to interlock.

CTA-ID : 5049
Was this helpful?
What can we do to improve the information ?