Technical FAQs

Ask a Question

What are the VA rating of the transformers in the C and D frame Omegapak 8804 CT, EVT and VTunits?

The VA ratings of the transformers are as follows:
300 VA for control
750VA for fans, precharge, etc.


CTA-ID : 4192
Was this helpful?
What can we do to improve the information ?