Technical FAQs

Ask a Question

Why doesn`t Omegapak 8804 CT, EVT and VT the drive run at 0 speed when the 0-10 volt signal is at 0?

The drive will run at 1.25Hz even when your speed reference is at 0. This is one of the Specifications on the drive.

CTA-ID : 4189
Was this helpful?
What can we do to improve the information ?