Technical FAQs

Ask a Question

What precautions should you take when going to add power factor correction capacitors to the system wih the Omegapak 8804 CT, EVT and VT drives?

If the power factor correction capacitors are going to be in the circuit all the time, you have nothing ot worry about. However if they are going to switching, may have to add line reactors on the front end of the drives.


CTA-ID : 4187
Was this helpful?
What can we do to improve the information ?