Technical FAQs

Ask a Question

What is part number for the 115 volt control power transformer for fans and precharge on the Omegapak 8804 1CFG-4R?

It is part number 30021-863-75, 500va transformer, primare 460/230/208 to 115 volt secondary.


CTA-ID : 4178
Was this helpful?
What can we do to improve the information ?