Technical FAQs

Ask a Question

Do we need to use one of the tubes with the XVAC00 conduit adapter?

No. It attaches directly to 1/2 inch conduit and the base of the XVA.


CTA-ID : 5034
Was this helpful?
What can we do to improve the information ?