Technical FAQs

Ask a Question

Is the 2510 KO1T one replacement switch or two?

One switch only, if both units need changing order two switches. This also applies to 2510 KO1AT, 2510 KO1BT, 2510 KO2T, 2510 KO2AT, 2510 KO2BT, and 2510 KO2CT devices.


CTA-ID : 4450
Was this helpful?
What can we do to improve the information ?