Technical FAQs

Ask a Question

What is the part number to replace the meter mounted on the door of the Omegapak 8804 CT, EVT and VT Omegapak in an MCC?

If it is an Analog meter then the part no. is AM-1 or if it is Digital then it is DM-1.

CTA-ID : 4174
Was this helpful?
What can we do to improve the information ?