Technical FAQs

Ask a Question

What is the part number for the 24 volt contol transformer on the Omegapak 8804 CT, EVT and VT?

The part number for the contol transformer is 30025-628-50.

NOTE: The part number printed on the unit may be MG1-15.


CTA-ID : 4164
Was this helpful?
What can we do to improve the information ?