Technical FAQs

Ask a Question

What is a XACB961?

It is the adapter for self supporting cable for a XACA pendant station. It consists of 2 screws that mount to the top of the pendant. These screws have holes in them to attach the cables from the self supporting cable.

CTA-ID : 5007
Was this helpful?
What can we do to improve the information ?