Technical FAQs

Ask a Question

What is the consumption of the control coil for 8502 SJ contactor?

1780 VA inrush and 48 VA sealed for 60 hertz or 1960 VA inrush and 59 VA sealed for 50 hertz, this applies for all electrically held voltages. 1530 VA inrush for 60 hertz or 1250 VA inrush for 50 hertz, this applies for all mechanically held voltages. This also applies to all 8536 SJ, 8538 SJ, 8539 SJ, 8606 SJ, 8630 SJ, 8640 SJ, 8702 SJ, 8736 SJ, 8738 SJ, 8739 SJ, 8810 SJ, 8903 SJ, 8940 S Size 7 except ``NP`` devices.



CTA-ID : 4700
Was this helpful?
What can we do to improve the information ?