Technical FAQs

Ask a Question

What is the cable that is just above tha fault lights from Omegapak 8804 CT, EVT and VT MCB to the serial communication, it is not ribbon cable but a buch of wires with a row of 18 pins?

Would need to get the serial communication kit MC16 for the serial communication cable.
It is J4 on the MCB.
The ribbon cable is 52011-047-52 that connects main control board to the option board.

CTA-ID : 4159
Was this helpful?
What can we do to improve the information ?