Technical FAQs

Ask a Question

Will the Omegapak 8804 CT, EVT and VT drive communicate with Modbus or Modbus +?

No. Not Directly. This drive only works with Symax SyNet communication.
There are some third party, non SquareD devices that can bridge from SyNet to Modbus and some other protocols. These devices would not become part of the drive but would simply bridge the SyNet to the desired protocol.

CTA-ID : 4156
Was this helpful?
What can we do to improve the information ?