Technical FAQs

Ask a Question

Is the Omegapak 8804 PF01 option adjustable?

The 8804 PF01 is not adjustable. It is a sealed device.


CTA-ID : 4151
Was this helpful?
What can we do to improve the information ?