Technical FAQs

Ask a Question

Can we use a XALB in NEMA 4 application?

The XALB enclosures have no NEMA ratings. They are rated IP65. This is IEC equal to NEMA 4.


CTA-ID : 4979
Was this helpful?
What can we do to improve the information ?