Technical FAQs

Ask a Question

Why can`t Omegapak 8804 CT 75hp with a C07 iso card achieve a span of 70 to 100%?

The option card is analog as well as the MCB input. The iso card would only allow for a 50 to 100% span. Some adjustments may cause the output signal to go above 2.5V.


CTA-ID : 4144
Was this helpful?
What can we do to improve the information ?