Technical FAQs

Ask a Question

What is the part number for the snubber resistors (PX1 4), GR870179, and ER870179 on the Omegapak 8804 1RCAAN?

The part number for the snubber resistors is 6703PX14.0. Do not know what GR870179 and ER870179 are--need a descirption. If they are mounted on the side with a diode, would be snubber assembly 52011-240-50.


CTA-ID : 4141
Was this helpful?
What can we do to improve the information ?