Technical FAQs

Ask a Question

Want the part number for the dc bus snubber resistor which is mounted on the back of the Omegapak 8804 ICV04T heatsink?

These resistors are part of the entire snubber assembly. However, the part number for the resistor assembly is 52011-184-51.


CTA-ID : 4140
Was this helpful?
What can we do to improve the information ?