Technical FAQs

Ask a Question

What is the part number for the door fan on the Omegapak 8804 CT (50-100hp), EVT & VT (60-125hp) ?

The part number is 26016-31100 for the door fan and these size units do not have a heatsink fan.


CTA-ID : 4139
Was this helpful?
What can we do to improve the information ?